STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! Unable to write to RAW Structur in MC Motor Pilot

Hello,I am trying to write to SPEED_RAMP using the Registers tab in MC Control Pilot, however I get the following error:ASPEP_RESP ERROR:ERROR_BAD_RAW_FORMATI am writing the data as follow for example: 6000;500Can someone help me find the right synth...

AnthonyK by Associate III
  • 820 Views
  • 1 replies
  • 0 kudos

Resolved! Motor Pilot (Observer + PLL) C1 / C2 Parameter Tuning

Hi all,I'm currently using Motor Pilot v1.2.12 and working with Observer + PLL mode for sensorless control. I see that there are parameters C1 and C2 available for tuning, but I'm not quite sure what each of them does and how they affect the motor co...

1123 by Associate II
  • 1009 Views
  • 1 replies
  • 0 kudos

Cannot generate the IDE project

Hi, Community.When I try to generate an IDE project from the MotorControlWorkbench project I inherited, an error occurs.I checked both cases where a previous IDE project existed and where only the stwb6 file existed, but neither worked.The IDE, MX, a...

hijimasa by Associate II
  • 1968 Views
  • 4 replies
  • 0 kudos

STSPIN32F0: Maximise PMSM motor starting torque

Demande de support pour maximiser le couple de démarrage du moteur PMSM avec la carte STSPIN32F0Bonjour,Je suis ingénieur software embarqué chez Actia Micromobilité. Je possède un moteur PMSM avec effet Hall pour vélo, que je commande avec la carte S...

seif1 by Associate II
  • 1952 Views
  • 5 replies
  • 1 kudos

Resolved! speed measurement resolution

Hello.I am currently conducting FOC (Field-Oriented Control) tests using the Motor Control Workbench with the Nucleo-G431RB board and the IHM08M1 power stage.My target speeds are 300 rpm and 150 rpm.However, when using Hall sensors with motors that h...

sjson by Associate
  • 1776 Views
  • 2 replies
  • 0 kudos

Resolved! HSO ADC config

Hi :[VERSION]: MCSDK 6.3.1I have some questions regarding the HSO ADC sampling configuration. I am currently using a custom PCB to validate the HSO algorithm with the STM32G431 chip. ADC1 and ADC2 are used to sample voltage and current separately. Th...

propu by Associate II
  • 2570 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.