STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! ADC selection for HSO sensing

Hello STIm trying to generate a HSO compatible FOC board using the STM32G747CEUx but I am not able to select the HSO option for Speed sensing.I've seen the requirement of using atleast two different ADCs for the current sensor and voltage measurement...

Motonaut by Associate
  • 595 Views
  • 2 replies
  • 0 kudos

Does the STEVAL-CTM010V1 support 115200 baudrate ?

Hello,      I use MCWB 6.4.0 & Motor Pilot 6.4.0, STLINK V3 MINIE.      Motor Pilot can not discover STEVAL-CTM010V1 board.      And  I find that MCU can receive datas at buadrate 1200 to 14400, but failed at 19200  or  more fast .      Does the STEV...

wcx8229 by Associate II
  • 823 Views
  • 2 replies
  • 0 kudos

stm32 motor workbench

merhaba topluluk. elimde bir adet f303re kartı ve bir adet ıhm08m1 kartı var.foc kontrol ile bir bldc motor sürmem gerekiyor. ancak bazı sorunlarla karşılaşıyorum.1)nominal deviri 1000rpm girdiğim halde motorpilot arayüzünde 2300rpm e kadar çıkıyor v...

X-NUCLEO-IHM05A1

for this motor controller  X-NUCLEO-IHM05A1. i downloaded zip file from website X-CUBE-SPN5. then after i tried implement with the stm32cubeide. i have a STM32Nucleof401RE microcontroller. I don't understand how to use this file can anyone please gui...

dhva1234 by Associate II
  • 657 Views
  • 2 replies
  • 0 kudos

Resolved! Programmer can't find STEVAL-ESC002V1

Hello,  I am using a STEVAL-ESC002V1 board and I am stuggling to make it work. I want to load the bin file given in STSW-ESC002V1 but the STM32Cube Programmer does not find the board. I am using a STlinkV3Minie connected to the SWD connector.The inst...

ifez by Associate
  • 1589 Views
  • 2 replies
  • 1 kudos

Understanding of Parameters in sto-pll

Hi ST,I am trying to understand sensor less speed measurement using STO-PLL observer I did not get any idea for the parameters F1, F2, gain1 and gain2 parameters from user manual (STM32 motor control SDK user manual) and software code too. could you ...

Rahuld_0-1751360567211.png
Rahuld by Associate III
  • 1304 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.