2025-01-20 12:48 PM
Hello,
I am using a STEVAL-ESC002V1 board and I am stuggling to make it work. I want to load the bin file given in STSW-ESC002V1 but the STM32Cube Programmer does not find the board. I am using a STlinkV3Minie connected to the SWD connector.
The instructions given to use the board are really rudimentary and I am new to ST work environment so I am a bit lost.
Is it a better option to use the bootloader? If so how do I do that?
I'll gladly take any help.
Solved! Go to Solution.
2025-07-06 10:45 AM
I found the problem! You have also to add the VAPP to you STLink (PIN 1 at STLink V2).
It's easy to solder a connection to C1 on the Board.
Have fun!
2025-07-06 10:02 AM
I have the same issue with STLink V2... Can't get a connection to the board. Did you find a solution?
2025-07-06 10:45 AM
I found the problem! You have also to add the VAPP to you STLink (PIN 1 at STLink V2).
It's easy to solder a connection to C1 on the Board.
Have fun!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.