STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! torque mode with hall sensor

Hello ST Community,I am currently using the EVSPIN32F0251S1 inverter board to control a BLDC motor in an elevator door control application.When I run my BLDC motor in torque mode and set torque with this api  MC_ProgramTorqueRampMotor1_F() so my moto...

Vedant07 by Associate II
  • 797 Views
  • 1 replies
  • 1 kudos

Resolved! Speed Loop PID Tuning in ESC001V1

For PID tuning, from documentation, I understood how to calculate gains for current loop. But how to calculate them for speed loop? How Motor control workbench is auto calculating the gains for speed regulator? Please provide documentation or formula...

How to cool B-D431B-ESC1

I saw in a post here that someone blew up their B-G431B-ESC1 with just 5As using the motor profiler. The spec says the mosfets will output up to 120A. I am looking to run motors up to 30A. I'd like to see if there is a prescribed way of adding heat s...

robomow by Associate II
  • 1000 Views
  • 3 replies
  • 0 kudos

Resolved! EVSPIN32G06Q1S3 not in CubeMX board selector

I'm trying to program the EVSPIN32G06Q1S3 to run a PMSM, but I attempted to use STM32CubeMX to help with the pinouts and code. The problem is that I can't find the EVSPIN32G06Q1S3 in the board selector. Is there a way to download then import the boar...

Hugo_ by Associate
  • 1020 Views
  • 2 replies
  • 0 kudos

Resolved! How can I configure the Motor with low speed

Hi, I'm working on a project in MC Workbench 6.3.2 and trying to configure a motor with a maximum speed of 150 RPM. When I set the "Max. Application Speed" parameter to 150 RPM (as shown in the first picture), I encounter an error related to the "Spe...

maxspeed.jpg sensor_setting.jpg
DF_MC by Associate III
  • 1741 Views
  • 6 replies
  • 2 kudos

MCSDK 6.4.0 Board Designer question

I dump a STEVAL-SPIN3204 board in STMC Board Designer and want to add "Electronic Speed Control" Feature.In Board Designer I had add this feature without error. But in Motor Control WorkBench as attached 1.JPG .We can see ESC feature. But in project ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.