STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! The starter motor failed to start

Dear ST motor control experts:      I am currently debugging a PMSM using MCSDK6.3.2, with the following components: MCU: STM32G473QET6, control board: B-G473E-ZEST1S, power board: STEVEL-LVLP01. However, the motor fails to start. Upon inspection, it...

Cannot connect to STEVAL-SPIN3204 board

The board appears in Device Manager on my Windows 10 PC, and port/baud rate/parity settings match what is in Motor Pilot and STM32CubeProgrammer. Neither Motor Pilot nor STM32CubeProgrammer will connect to the board. I am using the latest drivers. Wh...

sargross by Associate
  • 496 Views
  • 3 replies
  • 0 kudos

Torque control - speed feedback error

Dear Support team,I am currently working on a NucleoF302R8 and IHM07M1 driver to run a 24V PMSM motor (rated at 3600 RPM, no load).I'm using STM32 Motor Control Workbench version 6.4.0. Whenever I attempt torque control, I consistently encounter a sp...

Increasing sensored FOC encoder feedback loop

Hi,   I am trying to create an online angular velocity controller where my torque is dependent on the angular velocity of the motor (motor being driven by the plant). Basically, I want to resist the movement from the plant in a way that keeps the con...

KStew.1 by Associate III
  • 1059 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.