STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

"Can't compare values of these types. Allowed comparisons are between two numbers, two strings,..."

2025-08-12 10:04:37,611 调试 [WB_to_MX.lambda$run_gui_mode$0] 参数:[-mx_timeout, -1, -pack, assets/MotorControlPack/MotorControl.zip, -exp, templates/wb-defines_where_and_what.txt, -ftl, templates/wb_ioc_template.ftl, -xdm, E:\STMotorControlWorkbench\640...

EVSPIN32G06Q1S3 and STLINK-V3SET not communicating

I am working with the EVSPIN32G06Q1S3 and the STLINK-V3SET, I have the two programmer/debugger boards mounted on top of each other. Then I have the UART connector connected to the EVSPIN32G06Q1S3 (J5) and the programmer/debugger boards (CN7). I have ...

Hugo_ by Associate
  • 576 Views
  • 2 replies
  • 0 kudos

Resolved! Regular Conversion Manager MCSDK 6.4.0

I have manually migrated from MCSDK 6.2.0 to 6.4.0 for my micro STM32G431RBT6 from the example project as i have seen several changes in the source code and HAL drivers and i want to keep the project upto date for any future changes and can adapt eas...

STuser2_0-1754563002980.png
STuser2 by Senior III
  • 675 Views
  • 2 replies
  • 0 kudos

Resolved! custom STSPIN32G4- Dual motor, 2nd motor does not work

[PN]: STSPIN32G4[VERSION]: 6.4.0[TOOL]: Motor Control Workbench[DETAILS]:In this design, the second motor does not work as the interrupts that invoke the FOC_HighFrequencyTask by setting the motor ID into the array FOC_array[] are not enabled (TSK_Du...

GSB by Associate II
  • 728 Views
  • 3 replies
  • 1 kudos

MCSDK 6.4.0 Flux weakening problem

[PN]: EVLSERVO1[VERSION]: 6.4.0[TOOL]: MC Workbench[DETAILS]:Issue 1After enabling Flux Weakening, I can achieve higher motor speeds; however, under a constant load the speed sometimes swings dramatically. My observation suggests that the control fir...

YungPin by Associate II
  • 1088 Views
  • 4 replies
  • 2 kudos

Resolved! X-CUBE-SPN5 Installation

hello,I am a student, and for my university project, we are using this stepper motor controller X-NUCLEO-IHM05A1, and I have the STM32NucleoF401RE Microcontroller board to send the command to the motor control. I see there is one middleware package f...

dhva1234 by Associate II
  • 1313 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.