2025-07-31 5:02 AM - edited 2025-07-31 5:10 AM
Hello and good day.
When using my custom board, I am facing "The following has evaluated to null or missing" errors during code generation. I have tried a few variation of custom boards but I can't seem to solve the issue. FYI, this doesn't happen when generating code using ST evaluation boards.
Is this an issue from my side?
I am using the latest MCSDK v6.41 and STM32CubeMX 6.15.
I have attached my project file for reference.
Edit: I am using STMC Board Designer Version: 1.2.1 and I just uploaded the board design.
Solved! Go to Solution.
2025-07-31 5:49 AM
Hi fmariz, as described into the "known Limitations/For 6Step algorithm" section of the "Release Notes" for the ST MCSDK 6.4.1, the supported series for the 6step algorithm are the following:
Please refer to Release Note available through "Workbench tool">About>Documentations>Release Notes> link
Best regards.
Fabrice
2025-07-31 5:49 AM
Hi fmariz, as described into the "known Limitations/For 6Step algorithm" section of the "Release Notes" for the ST MCSDK 6.4.1, the supported series for the 6step algorithm are the following:
Please refer to Release Note available through "Workbench tool">About>Documentations>Release Notes> link
Best regards.
Fabrice
2025-07-31 11:44 PM
Thanks for the confirmation. I hope ST will remove the limitation in the next release. Also I hope that STM32H523 series will be added into the supported MCU list in the Board Designer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.