2025-07-31 6:23 AM
Hi everyone,
I'm using MCSDK v6.4.0 with an STM32G4, a 42BLF01 motor, and a high-quality incremental encoder with Z-index.
My goal is to accurately correct the electrical angle on each Z-pulse to avoid long-term drift after 100 rounds.
In previous SDK versions, there was a function called ENC_SetElAngle() which allowed setting the electrical angle directly.
In MCSDK v6.4.0, however, this function no longer exists – and the corresponding enc_driver.h file is also missing.
Is there any official or recommended way in MCSDK v6.4.0 to directly set or correct the electrical angle at the Z-pulse – without using ENC_SetElAngle()?
If not:
What’s the recommended strategy for drift-free synchronization while the motor is running?
Is MC_SetCtrlPositionAngle1() the intended method – even though it may cause stepping or jitter?
Thanks for any insights
2025-08-04 1:31 AM
Hello @Baumi,
Which version are you referring to for "previous SDK versions"?
The ENC_SetMecAngle() function is available in the encoder_speed_pos_fdbk.c file located in the Project\MCSDK_v6.4.0-Full\MotorControl\MCSDK\MCLib\Any\Src directory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.