STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! My question is : can the C produced by the ST Motor Control Workbench be modified by to permit all 3 inverter currents to be measured by the same ADC, for example ADC 1? This would result in a 200ns delay for the 2nd measurement, and 400ns delay for 3rd

Messieurs,I am using the ST NUCLEO-F303RE together with an X-NUCLEO-IHM08M1 and the ST Motor Control Workbench (STMCW) to drive a BLDC motor using ST code.In addition, my company has designed its own motor control board for driving two BLDC motors us...

PBroo.2 by Associate
  • 1924 Views
  • 3 replies
  • 0 kudos

Resolved! Can I use Position control with Hall Sensor with SPIN-3201?

Hi, I am new to the Motion Control system.and I have SPIN-3201 with a BLDC motor.It is hard to apply ST Motor Control Workbench 5.4.6.because the version of STM32CubeIDE and some Setting of the Project(error of FOC duration and Start-up failure)anywa...

LYS by Associate II
  • 2792 Views
  • 4 replies
  • 0 kudos

Start a motor with sensor (using hall sensor) under heavy load situation, the motor will produce noise and motor sometimes can't move successful

I use MCSDK 5.3.2 and our board(which is similar IHM08h but we modify the over current from 30A to 60A) with using hall sensor to drive motor(our purpose is to drive E-bike and E-Scooter)But i find that in heavy load situation,i will hear motor will ...

SkyWork by Associate III
  • 1904 Views
  • 3 replies
  • 0 kudos

How to configure MCSDK for multiple motors?

Hello. I have done position control of single motor using P-NUCLEO-IHM03 with GM2804 + AS5048a(pwm encoder). And I hope to control 3 motors for gimbal. So I'm planning to design a board using the MCU and motor driver which are used in the P-NUCLEO-I...

wJang.1 by Associate II
  • 1640 Views
  • 2 replies
  • 0 kudos

Resolved! Relation between *.stmx file and drive_parameters.h ?

Often I find that MCSDK does not have the exact MCU I need to use so I need to end up modifying the CubeMx *.ico file generated from MCSDK.In trying to determine the relationship of these files I took an existing working project and renamed the *.stm...

BTrem.1 by Senior II
  • 1609 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.