STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! MCSDK: ICS gain range is 5V but ADC only works with 3.3V

Hi! I am using F746ZG + IHM08M1. And I need configuration with 2 insulated current sensors.My question is why in Workbench ICS gain is in range from -5V to 5V where the ADC max working range ist only 3.3V. Which current sensors should I buy 3.3V or 5...

VKost.2 by Associate II
  • 2285 Views
  • 3 replies
  • 0 kudos

Resolved! EVSPIN32F0601S3 High Voltage BLDC Motor Drive:

Hi,1) How to run demo code for EVSPIN32F0601S3 (As parameters attached) ?2) When I have EVSPIN32F0601S3 eval board with me do I need only Enter Motor Parameters as in mcsdk to spin the Motor  (As parameters attached) ?Thanks in advance..--Karan

MCSDK Motor phase sensing peripheral pin selection question ?

Hi everyone,I have a question about MCSDK for STM32G474QE mcu.I chose STM32G474QE in MCSDK gui software. My hardware phase sensing pins are connected to ADC1_IN5 (PB14) and ADC1_IN15 (PB0) pins. I want to use these pins for 2 insulated current sensor...

0693W00000APOmsQAH.png 0693W00000APOn7QAH.png
HK by Associate II
  • 1342 Views
  • 2 replies
  • 1 kudos

Resolved! Hi there, i am trying to get my STEVAL SPIN3202 running. I follwed the "Getting started"-Guide and got to the point where i have the Project in my STM32CubeIDE. When i try to build the project i have several errors: see in details

../MotorControl/mc_config.h:24:10: fatal error: pid_regulator.h: No such file or directory..\MotorControl\mc_config.h:24:10: fatal error: pid_regulator.h: No such file or directory..\MotorControl\mc_math.h:28:10: fatal error: mc_type.h: No such file ...

MM1 by Associate II
  • 1801 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.