2021-01-28 11:33 PM
Hello.
I have done position control of single motor using P-NUCLEO-IHM03 with GM2804 + AS5048a(pwm encoder). And I hope to control 3 motors for gimbal. So I'm planning to design a board using the MCU and motor driver which are used in the P-NUCLEO-IHM03
But, it seems that MCSDK does not support for multiple motor.
How can I set the basic IDE project for 3 motors?
2021-01-29 12:28 AM
I set IAR project for single motor control project using MotorControl Workbench 5.4.5
2021-06-01 1:49 AM
The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 SDK).
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.