STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! Start a motor with heavy load

Hello everybodyI'm using MotorControl Workbench and Motor Control SDK 5.4.1.I need to control some power tools up to currents of 40A peak. I developed a board similar to IHM08M1 and I'm very satisfied of the power delivered to motors. There's only a ...

EVALKIT-ROBOT-1.

How I can programming MCU (Example code with description, PID control, use STM32 Motor control SDK5.0, Motor control workbench and others)? Where is video example, AN?

Setting engine control modes in the FOC SDK

Hello colleagues! In the process of working in FOK SDK 4.3 with the controller STM32F302RE, I had several questions:1) When using the HFI mode, I can not configure the control settings. Perhaps you have some kind of guide to configure each parameter....

ABush.2 by Associate
  • 1910 Views
  • 3 replies
  • 0 kudos

SWST-ROBOT-1 fails to build in STM32CubeIDE V1.3.0.

The steps to reproduce: Uncompress STSW-Robot-1, import EVALKIT_ROBOT_1_SDK543_Positioning_LL.ioc using all default options. Answer ‘Yes’ to “Open Associated Perspective?�?Project Manager Settings appears, informs that “The Firmware Package required...

STM32CubeMX error loading existing project

"Can't Add: MotorControl files not found"This above is the error I get when I try to load an existing project using STCubeMX V5.6.0.My toolchain set up works on my laptop and I attempted to duplicate the same tools on my work computer. Both are Wind...

BTrem.1 by Senior II
  • 2103 Views
  • 4 replies
  • 0 kudos

Resolved! Why are Regular Conversion Manager (RCM) functions not present in the MC SDK 5.4.3 code while present in the documentation?

Hi,I am develloping a system using the motor control sdk. I am usiung the ‎STSPIN32F0‎ chip and the following software versions:This module only has one ADC peripheral and I need to use it in my application. Looking around, I have found that the Regu...

0693W000000Wl3fQAC.png 0693W000000Wl3uQAC.png 0693W000000Wl4YQAS.png 0693W000000Wl4iQAC.png
PBela.1 by Associate II
  • 3029 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.