2019-12-12 5:50 AM
Hello everybody
I'm using MotorControl Workbench and Motor Control SDK 5.4.1.
I need to control some power tools up to currents of 40A peak. I developed a board similar to IHM08M1 and I'm very satisfied of the power delivered to motors. There's only a "little" problem: I should improve the behavior at heavy loads when motor has to startup, because I noticed that in this case it fails to start. I've a linear ramp of 750ms in which motor moves from 0 rpm to 1650 rpm (15% of nominal speed at free load) and the final current in this phase is the nominal current (so the max current we can give to the motor).
Could be a practical solution create a phase in which current rumps up very quickly to nominal value and desired speed moves from 0 rpm to a little value in a brief time? After that phase I would add a phase in which current is still constant at the maximum value and speed moves from the previous little value to the 15% of nominal speed to exit from open loop mechanism.
Did anybody try a solution like this? Or maybe there's a better way?
Thank you very much for support.
Roberto
Solved! Go to Solution.
2020-01-23 6:38 AM
2020-01-17 5:32 AM
Hello Roberto,
are you using sensored or sensorless solution?
Thanks,
Claire
2020-01-17 6:30 AM
Hello Claire
I'm using a sensorless solution.
Thanks
Roberto
2020-01-17 6:54 AM
ok, this explain your current problem Roberto.
There are no trivial answer to your question ... our solution is not tuned today to support heavy load at low speed.
But, we are working on this point and some progress are expected this year on this point.
Please stay tuned...
Claire
2020-01-17 7:03 AM
Ok, so in your opinion there's no way?
Or maybe I can try to obtain some results If I slighly modify parameters? I can't work on it until my own board is finished, so I'm only thinking about it, at this time.
Roberto
2020-01-20 11:13 PM
Dear Claire,
just another question: if I use Hall sensor, does this solve the question?
Thank you for support.
Roberto
2020-01-23 6:38 AM
yes, it should improve the torque level at low speed.
Thanks,
Claire
2020-04-28 7:42 AM
Dear Claire
Can you tell me if there are some good news about my "problem"? Did Motor Control Suite introduce some improvements for solutions sensorless?
Thank you so much
Roberto
2020-09-22 4:03 AM
Dear Roberto Giovinetti
We will probably make some announcements about sensorless solution support in 2021.
Do not hesitate to contact us again at this time.
Best regards
Laurent C.
2021-01-26 5:28 PM
Hi @Claire OKU
is there any way to solve sensor mode (I using hall sensor to start motor)?
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.