STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

How to measure RPM with STEVAL-ESC002V1?

I succeeded in operating the Tartget Motor with STEVAL-ESC002V1.However, since the STEVAL-ESC002V1 is not linked with'Motor Profiler 5.4.4' SDK, it is impossible to check the motor operating speed.​I know that STSPIN32F0A has a function that can meas...

WSeun.1 by Associate
  • 2092 Views
  • 5 replies
  • 1 kudos

Resolved! Over current protections by pass in steval 3202

hi sir i am using motor control workbench generated foc sdk and running motor of 6 pole bldc successfully but in my application of motor heavy load is given on motor so it indicate over current fault so please guide me to by pass overcurrent fault fr...

Ryada.1 by Associate II
  • 1666 Views
  • 2 replies
  • 0 kudos

Motor becomes unstable at 1200 RPM and stops with the P-NUCLEO-IHM001 Motor control Kit and Motor Control SDK 5.4.4 .

I am using the P-NUCLEO-IHM001 motor development kit Hardware: Microcontroller Board: NUCLEO-F302R8Driver Board: X-NUCLEO-IHM07M1Motor: Bull-Running model BR2804-1700 kVSoftware:Keil uVision 5 IDEST Motor Control Workbench 5.4.4Motor Control SDK 5.4....

0693W000006GNQhQAO.jpg 0693W000006GNRGQA4.jpg
AKhar.3 by Associate
  • 1731 Views
  • 3 replies
  • 0 kudos

Error : foc duration

Posted on November 28, 2012 at 09:29Hello, I'm working with foc sdk v3.2, I don't find in user manual um1052, the cause of error ''foc duration''. Thank you, Jean

Need Help for STEVAL-IHM042V1 board

Posted on February 09, 2016 at 20:09Hi,I am using STEVAL-IHM042V1 evalution board. But not found any library for that.I got MC FOC SDK which generate .h files.I will need .c Files as well.Can any one have so i can proceed further. #steval-ihm042v...

SS.Sagar by Associate III
  • 764 Views
  • 1 replies
  • 0 kudos

Current sensing with inverting amplifier

Posted on September 15, 2016 at 23:22Hi,I have been trying to use FOC SDK 4.2 with existing hardware. The board uses inverting amplifier instead of non-inverting ones. Anyone got an idea on how to modify the code?So far I've tried:1. use negative va...

ztymyws by Associate
  • 1489 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.