STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Stimulate error on motor

I use Lib version 4.3 to control SM-PMSM.The motor can run smoothly.However I would like to simulate 2 error hereafter.SW error (FOC Frequncy cannot be sustainable)Start up fail.I would like to check these 2 error without modify code. PS.I have lock...

JRoja.16 by Associate
  • 1007 Views
  • 1 replies
  • 0 kudos

Motor start vibration problem

I use FOC+Hall sensor(STM32F030RE MCU, ihm08m1 power board, MC lib 5.3.2).I try to start motor using MC_ProgramSpeedRampMotor1() function, but the e-bike has "start vibration" problem.How to avoid this problem? adjust pid or something else?any sugges...

cyt by Associate II
  • 1296 Views
  • 1 replies
  • 0 kudos

Question for Motor Control Firmware FOC V2.0

Posted on January 22, 2014 at 23:51Hello, Does anyone know where I can find the Source Files for the ''MC_FOC_Methods_lib.lib'' and ''MC_State_Observer_lib.lib''?There are parts of the open source code in the library files, where you can not look in...

hans by Associate
  • 1897 Views
  • 4 replies
  • 0 kudos

Absolute Encoder for St Motor Control library

Dear,I know that ST Motor control library does not support Absolute encoder, so I am trying with some difficulties to do it, I connected my motor with HALL sensor and also connected my absolute encoder with SPI, I can read the abs position without an...

JEsca.1 by Associate II
  • 2480 Views
  • 3 replies
  • 0 kudos

Using IHM001 to run a bullrunning motor

Posted on January 15, 2016 at 04:05Hi all,I am using IHM001,FOC4.2 to run a bullrunning motor. But a 'speed feedback' error always occurs when the motor runs below 1000 rpm.I have tried to chane some parameter, and the lowest speed can drop to 500 r...

yaojb by Associate
  • 2110 Views
  • 4 replies
  • 0 kudos

STM-FOC motor control

Posted on June 07, 2017 at 19:57Hello,We are a startup developing motor control solutions and our advanced motor controller is capable of controlling upto 8 motors simultaneously. We are planning on using STM’s sensorless FOC control methodology f...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.