STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

STM32 FOC PMSM SDKv3.0 & GNU arm-none-eabi-gcc

Posted on January 23, 2012 at 01:11I figured out some troubles during the migration of the FOC-library to the arm-none-eabi toolchain: The toolchain uses 32-bit wchar_t, but the library is compiled with 16-bit wchar_t. I'm not shure if this is the r...

clemens2 by Associate
  • 1401 Views
  • 4 replies
  • 0 kudos

FOC Library v4.3 available???

Posted on October 03, 2016 at 17:37I see in RN0085 that the FOC libary v4.3 is listed.  In new features for v4.3 I see AC6 workspace.  Yay! this is great for us.  We want to use the STM32 Open Development Env. as a base for all our firmware.  Pleas...

ICS and F303?

Posted on February 27, 2018 at 10:19In UM1052 it says that ICS current sensing is only available for F103 HD, F2xx, F4xx. However the class ICS_F30X_PWMnCurrFdbk is part of the MC Library. Is this class with it's functionality a work in progress? It...

freppa by Associate II
  • 976 Views
  • 1 replies
  • 0 kudos

How to configure for dual motor feedback

Posted on December 11, 2014 at 16:05Hi, I am trying to use the FOC4.0 library with dual rotor angle feedback, namely hall plus encoder. I can set this configuration via the GUI (I have to manually edit the generated header files because of a bug in ...

problem in compiling code using stsw-stm32100 library

Posted on February 06, 2015 at 19:36hello every body,i generated header files using MC workbench, and then copy them into sys_drive_param folder. then when i open workspace in project folder. it contains only STM32F30x_userpoeject, but according to ...

ijhar09 by Associate
  • 1955 Views
  • 5 replies
  • 0 kudos

Single motor on ADC3/4

Posted on March 11, 2015 at 22:52Hello,Does the PMSM FOC library support single motor drive using OPAMP3/4 and ADC3/4 on STM32F303RB?I did my own HW like that but it seems that the library still tries to check some flags of ADC1 even if none of the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.