STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Sampling 3 phase current with only 1 ADC

Hello,In motor control pack P-NUCLEO-IHM001, microcontroller is STM32F302R8 which has only 1 ADC.The motor drive has option to use 3 current shunts.By analyzing the datasheet, ADC does not have multiple sample & hold circuits.So, how would it be poss...

MMila.3 by Associate
  • 1567 Views
  • 3 replies
  • 0 kudos

Cannot build generated code

After generating the project with Motor Control workbench and building it on CubeIDE, I get this error : 15:10:13 **** Incremental Build of configuration Release for project Noname ****make -j4 all arm-none-eabi-gcc "../Src/aspep.c" -mcpu=cortex-m4 -...

Rced.1 by Associate
  • 1654 Views
  • 3 replies
  • 0 kudos

Problem with certain STMCWB parameter combinations

Posted on October 27, 2014 at 09:49Hi Gigi, I have a motor with rather unusual electrical parameters (low inductance, high number of poles, very high electrical rpm), and the generated output files for these settings are not usable. The compiler co...

HFI with STEVAL-IHM042V1

Posted on March 25, 2015 at 13:38Hi, I like to test the HFI function on the STEVAL-IHM042V1. Without HFI is the motor running well. But how can I implemented the HFI? I followed the instruction of UM1052 page 65. But I can not configure the DAC in t...

STM3210E-EVAL motor control example

Posted on January 18, 2012 at 17:00Hi, I'm trying to get a motor control example running on the mentioned board - without success. My main function looks like this: int main(void) {   SystemInit();   Demo_Init();   //initialize motor control lib  ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.