2014-01-22 2:51 PM
Hello,
Does anyone know
where I
can find the Source Files for the''MC_FOC_Methods_lib.lib'' and ''MC_State_Observer_lib.lib''
?There
are
parts of the open
source code
in
the
library files
,where you can not
look
inside.
Can someone
send
the source
files
for
me?
2014-01-23 6:46 AM
Ciao Hans,
Both MC_FOC_Methods and MC_State_Observer are protected parts of the motor control code. It can be released for free just after signing an appropriate ''Non-disclosure agreement (NDA)'' with ST. If you require it please contact your nearest ST office. Ciao Gigi2014-03-24 10:19 PM
Dear Gigi,
I am using a
STM32103VBT6 and STM32 PMSM FOC based BLDC program.
It works very well when it
drive a 16 inch hub BLDC motor(56 poles), but it has problems when driving a 14 inch (46 poles) hub BLDC motor whose speed is less than 60RPM.
It is unsmooth at low speed. The motor will produce large torque ripple
when hall sernsor
.
It also works well when
run
ning
at high speed.(>5km/h)
Can you tell me how to adjust
the
program to
14 inch hub BLDC
motor?
ThanksAlenEmail: xmgatech@gmail.com2014-03-31 1:16 AM
Ciao
URL :
/92e3f1c8
2021-06-28 3:03 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.