2018-09-11 8:13 PM
I use Lib version 4.3 to control SM-PMSM.
The motor can run smoothly.
However I would like to simulate 2 error hereafter.
I would like to check these 2 error without modify code.
PS.I have locked rotor when start ,it shows under-power error instead of Start up fail.
2021-06-28 3:06 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.