STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! STEVAL-SPIN3202. Got it turning. Now need a guidance on where / what file and how I can control the speed.

Hi All,Got it turning. Now need a guidance on where / what file and how I can control the speed. SDK 5.4.8.6S_STEVAL3202_SL_VM example.Monitor connects well.I can start the motor.Final ramp speed does not work. The only use - setting the direction of...

EShaw.1 by Associate II
  • 9133 Views
  • 19 replies
  • 0 kudos

Is it possible to remove PID from BLDC 6 step SDK

Hello, I am working on a project that requires control the motor speed by adjusting bus voltage. The PWM width shall be consistent. The motor bus voltage is controlled by another ST micro. Is this a possible approach? What documents/ examples I can r...

YWang.15 by Associate II
  • 818 Views
  • 0 replies
  • 1 kudos

Resolved! F401RE + IHM16M1

HelloI am using the combination of F401RE and IHM16M1 for a project in my lab to drive a 24V BLDC Motor (max RPM 5000). Issues:1) I am unable to select the above combination in the Motor Profiler.2) When I try to generate code using Motor Control Wor...

0693W00000QNbhCQAT.png
AChha.1 by Associate II
  • 8089 Views
  • 14 replies
  • 0 kudos

Resolved! MC SDK not work with MCU Stop mode

Dears,Currently I'm working on a BLDC project, and with the MC SDK, we can control the motor.And we also want to make the MCU(STM32F4) into STOP mode to save some power, the issue is the MCU can not goes into STOP mode, anyone tried this before?​The ...

0693W00000Sv4dmQAB.jpg 0693W00000Sv4dwQAB.jpg
Guopeng by Associate II
  • 10268 Views
  • 10 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.