2021-05-14 2:54 PM
My company produces systems that use very high resolution optical encoders, with over 2^16 quadrature counts per rev (over 2^14 PPR). We are looking to modernize our positioner electronics and have been prototyping with a NUCLEO-G431RB and an IHM07M1 in 3-shunt mode.
When entering our motor parameters into the MCSDK, I can enter e.g. 20,000 for "pulses per mechanical revolution". In the generated code, M1_ENCODER_PPR holds this value. However, ENCODER_M1.PulseNumber, which is a uint16_t, is set to 4*M1_ENCODER_PPR (presumably this is CPR and the 4x comes from quadrature decoding). This value will be truncated when M1_ENCODER_PPR is greater than 16,383. All of our systems exceed this PPR threshold, so we can't use the MCSDK as-is.
So to summarize, there are a few directly related issues:
I was actually able to overcome this limitation somewhat by dividing the pole count and PPR by e.g. 2 in the MCSDK, then also dividing the reported angle (wMecAngle, which is an int32_t) by 2 before it is fed into the position controller. This isn't really ideal, however; is there a better supported/recommended way to do this?
2021-05-16 5:48 PM
High resolution encoders are pretty common these days and your control algorithm has to use the appropriate variable type. I'm not sure why the MCSDK would use a uint16_t (maybe it was written for an 8 bit device?), seems like all the math should be done with unit32_t and if you're doing positioning loops where the encoder counts accumulate, you might need uint64_t. If it was me, I'd just make all the integer types in the control algorithm uint64_t if I could.
2022-04-06 8:51 AM
I was disappointed to see that version 6.0 of the MCSDK is still using uint16_t.
2022-09-27 4:15 AM
I've experienced the same issue and ended up having to truncate the 2^19 bit position down to 14 bits to ensure it fits in the 16-bit registers. I looked at changing the 16-bit variables to 32-bit values but the entire SDK is just a complete mess and the inter-dependence between variables is all mostly undocumented so the attempt failed miserably. Just a gripe but I've been trying to get a high-res encoder running for a month now with no luck, there's just too many bugs in the SDK to make it reliable. Just my penny's worth, sorry.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.