STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! MCSDK 5.Y.3: no electrical speed and no speed control with quadrature encoders, but behaves like position control

Hello,I struggling with MCSDK 5.Y.3 to control a 24V, 15 poles pairs, 300 rpm hooverboard-style BLDC motor, nearly no load, with a Nucleo F401 and a IHM08M1 power board.I try to use FOC control with 526 PPR quadrature encoder as main sensor as I want...

Resolved! For the B-G431B-ESC1, what is the pitch of the J5 header?

It's cool that the schematics are available, and the assembly drawings are ok.but a full set of gerbers with all the traces and pads would be much better, esp. if it were in an EDA agnostic format.In lieu of that, what is the pitch of the J5 pads?

GHave.1 by Associate II
  • 2202 Views
  • 3 replies
  • 0 kudos

[Bug Report MCSDK 6.0.0] Overvoltage and overcurrent flags inverted when overvoltage protection is disabled

Hello,Actual behavior:While I have deactivated the overvoltage protection in Motor Control Workbench, I still get the overvoltage fault flags that is sometimes set (when my motors brakes abruptly).My setup: 4-poles BLDC motor, MCSDK 6.0.0, Nucleo G47...

0693W00000SwMPfQAN.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.