STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

EVSPIN32G4 - Hall (H1 on PB6) is being pulled to ~2V

Hello - I've generated a few test projects in the ST Motor Control Workbench using the default settings and my motor's parameters. I've enabled the Hall sensing on TIM4 using PB6, PB7, and PB8. Those three pins are broken out onto J6 of the EVSPIN32G...

Motor Profiler 5.4.8 and Maximum Speed

Hi,I am using motor profiler 5.4.8 with F302R8 and IHM08M1 to get the motor profile of my BLDC motor.I have a query. Let say the maximum speed i get from the motor profiler is 30krpm. Can i change the maximum speed in motor control workbench (e.g. fr...

KToo.1 by Associate
  • 1375 Views
  • 1 replies
  • 0 kudos

We are using EVSPIN32F0251S1 Motor Control board. We are able to drive the lower mosfets on the board , however we are not able to drive the higher side mosfets.

We think the firmware configuration is correct because we tested the same code on STM32F0 discovery board and PWM gets generated on all the 6 pins which are used in the EVSPIN32F0251S1 board.So code is not issue. Can anyone explain what can be the a...

PShah.4 by Associate
  • 2027 Views
  • 3 replies
  • 0 kudos

STM32G4 and TMC2209 example project

Hi​I need to control a stepper motor with TMC2209 driver from my STM32G4 project but I cannot find any examples to start with.​I am new to embedded programming and this is turning harder than expected. I have been trying for more than a week now with...

RPG by Senior
  • 1107 Views
  • 0 replies
  • 0 kudos

pin level when disabling pwm

I'm using a general-purpose timer to generate low level pulses, configuring one channel as PWM. The problem is when I disable the channel, the signal goes low, and I want it to remain high.I played with the OCPolarity and PWM modes 1 and 2, but only ...

DAlvarez by Associate II
  • 3661 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.