STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

Resolved! X-NUCLEO-IHM01A1 and development board

Hi STM,I am having NUCLEO-476RG and I am planning project with steppers (by using X-NUCLEO-IHM01A1). Can I connect this expansion with my development board. And also, what is the maximum number of expansion boards I can connect to the development boa...

akara.31 by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

Resolved! Motor does not start with B-G431B-ESC1 board.

Hi all,I'm new to the STM32 world and ST motor control tools, so I might be missing something obvious.I have the B-G431B-ESC1 development board connected to a BLDC motor.I generated the code for FOC with the MC-WB 6.1.2 and STCubeMX 6.8.1. Compiled w...

_legacyfs_online_stmicro_images_0693W00000blAX7QAM.png

Resolved! How to access STM FOC FW library?

Hello!I would like to use the STM32 PMSM FOC firmware library. According to the release note of the SDK (https://www.st.com/content/ccc/resource/technical/document/release_note/b1/3f/4e/1b/cc/7f/45/c1/DM00068242.pdf/files/DM00068242.pdf/jcr:content/t...

EAbraham by Associate
  • 4985 Views
  • 1 replies
  • 0 kudos

STM32G431 shunt + opamp + comparator network values

I have changed the G431-ESC-1 shunt resistor to 0.001ohm, and gain network resistor values as attached pics, for 100A phase current max with 1mOhm shunt resistor after the off-set circuit, the voltage is 0.19V to comparator's + input (non-inverting) ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.