STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

High Dynamic Low Ripple Setup

Dear forum,For my research project I need to generate arbitrary torque spectrums. Ideally with frequencies of up to 3.5kHz. I planned on using a ~200W PMSM and am now wondering which STM microcontroller and motor control board would be best suited fo...

MaxZ by Associate
  • 3601 Views
  • 1 replies
  • 0 kudos

PWM complementary Output

Hi,I try to implemend sinus algorithm for BLDC engine on  STM32G474RE chip.  I want to use TIM1 (CH1 - CH3) and (CH1N - CH3N) to control a bldc controller. I have configured a complementary output with dead time according to datasheat (so I think) an...

Screenshot from 2023-07-06 14-59-22.png Screenshot from 2023-07-06 14-59-31.png
Arek by Associate
  • 1197 Views
  • 0 replies
  • 0 kudos

Resolved! Hall Sensor - ST MC WB

I successfully ran the BLDC hub motor with sensorless method (sensorless + PLL) with EVSPIN32G4 hardware. My motor have the inbuilt hall sensor with 60 degree placement. Now, I am trying to configure with hall sensor. I get the speed feedback error i...

prasanthkumar22_1-1688561632862.jpeg prasanthkumar22_2-1688561937296.jpeg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.