STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! B-G431B-ESC 6-step algorithm breaks at @2KRPM

Hello, I'm trying to use my B-G431B-ESC with the 6-step algorithm. I''ve tried with a coupld of profiled motors and what happes is that it starts up fine, but after ~2K RPM, the motor starts to squeel and lose power. I feel like this has something to...

sgordon777_0-1702058349775.png sgordon777_1-1702058383770.png

Resolved! B-G431B-ESC1 HardFault with MCW generated code

I generated some code with the default "Electronic speed control on B-G431B-ESC1 kit" project in Motor Control WorkBench.  Then when I flash the default code I get a HardFault when calling `__HAL_FLASH_PREFETCH_BUFFER_ENABLE()` in  `HAL_Init()`:int m...

B-G431B-ESC1 sensorless example just makes motor beep

I'm trying to use the dev kit to run a BLDC motor in sensorless mode using the default MCW project.  When the motor starts up I hear a high pitch chirp and then the firmware repeditively tries to spin the motor which results in more periodic chirps. ...

Unable to download SDK

I can't seem to download any software from the ST website.Whether it's the MC SDK or even just the STM Cube programmer. The download button is there when I'm logged out, but all the links disappear once I log in. Alternatively, if I request a downloa...

Resolved! NUCLEO-H753ZI and Motor Control WorkBench

Hello,I try to use the NUCLEO-H753ZI in combination with the Motor Control WorkBench 6.2.0.Unfortunately, the bord isn’t supported out of the box now.My experiments to define a new bords runs in several errors.Is there a way to use the STM32H753ZI wi...

albHW by Associate
  • 1377 Views
  • 1 replies
  • 1 kudos

EVSPIN32F06Q1S1 Questions?

Hello all.I am new to motor controllers and have some questions as I try to understand drivers for BLDCs.I am looking to drive a compressor (using BLDC motor driver).  I require up to 400V at about 2.5A (so 1000W max power).It seems that I could do t...

SWenn.1 by Senior III
  • 3140 Views
  • 4 replies
  • 0 kudos

doubt regarding STEVAL-SPIN3201

Still facing problem in STEVAL-SPIN3201. I  got errors like FOC  duration and software error. unable to start the motor. May i know what is the problem?I decreased PWM frequency, changed the execution rate, changed the PID values. Still the errors ar...

vishu by Associate II
  • 4644 Views
  • 3 replies
  • 0 kudos

Resolved! Motor spin without Motor Pilot program

Hello,I'm very biginner.By MCSDK6.2, I generated code and tried to spin 3 phases BLDC motor with code" MC_PrgramSpeedRampMotor1(1725, 2000);" and"MC_Startmotor1();"I inserted these code and built and tried to run, but it didn't work.The motor didn't ...

화면 캡처 2023-12-11 145920.jpg 화면 캡처 2023-12-11 145850.jpg
yourbryan by Associate II
  • 2827 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.