STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! Board Manager Phase Voltage Generation difference

I am currently going through the documentation of the Board Manager.What was not clear to me is the difference between the Phase Voltage Generation settings DrivingHighAndLowSides and PoweringHighAndLowSides.It does not help that the latter doesn't h...

DMeie.2 by Senior II
  • 1528 Views
  • 1 replies
  • 1 kudos

EVSPIN32G4-Dual driver 2 motor issue

[VERSION]: MCSDK 6.2.0[TOOL]: MC WB,[DETAILS]: PWM output Abnormal [EXPECTED BEHAVIOR]:M1 & M2 should drive independently & smoothly[HOW TO REPRODUCE]:1.Profile M1 & M2 by Motor Profiler with EVSPIN32G4. M1 & M2 got Hall .2.Use MCSDK 6.2.0 with EVSPI...

BLDC Motor not Starting Properly

I am making a BLDC motor controller using STM32G0 microcontroller. The commutation technique that I am using is SVM. But during the initial start, the motor is not rotating properly (vibrating back and forth), It can be seen in the following image wh...

starting issue.png
Gladson by Associate III
  • 1692 Views
  • 1 replies
  • 0 kudos

STM32 Nucleo FOC adn 6-step motor control firmware

I'm just getting started with the above kit - first step was to reprogram the board to blink the LED! Now I'd like to controlling the motor. I see instructions to reprogram the .bin file, but I was expecting to see an example program with source code...

dnajemy by Associate
  • 1138 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.