STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! Servo buzzing and not working with STM32G030C8T6

Hi, I encountered a problem while trying to control servo motor(SG90) with my custom STM32G030C8T6 board. Servo is not moving at all and only buzzing quietly. I am supplying servo from 5V, board and servo have same GND. I checked servo power supply w...

MaciejG_0-1701631594463.png MaciejG_1-1701631675575.png MaciejG_2-1701631725500.png
MaciejG by Associate II
  • 3507 Views
  • 4 replies
  • 1 kudos

Resolved! B-G431B-ESC1 kit not working well

I've purchased a B-G431B-ESC1 kit and loaded it up with software (Details below)and soldered Phase, Power, and PWM/+5/Gnd wires.A couple problems and questions: -On most of my motors, there is no motion produced just some clicks, even though I've mat...

Problem with Motor profiler

[VERSION]: MCSDK 6.2.0 [TOOL]: Motor PROFILER v1.2.4EVALSTDRIVE101 + NUCLEO-F746ZG [DETAILS]: I have a sensorless project which work perfectly when the motor profiler option is disable. however, when the motor profiler option is enable, either the pr...

backb0ne by Associate II
  • 4157 Views
  • 5 replies
  • 0 kudos

Resolved! B-G431B-ESC1: How to build software?????

All I want to do (for now) is build the ESC software and download it into the B-G431B-ESC1 board.1. After alot of searching, I installed this: MC_SDK_6.2.02.  I ran MotorControl Workbench 6.2.0, loaded the "Electronics Speed control on B-G431B-ESC ki...

sgordon777_0-1701847684750.png

Manual to configure hall/quadrature sensors in CubeMX

I am quite a bit dissapointed, that it is not enough to have the following things:- datasheet- reference manual- application note 4013 "cross-series timer overview"- cubeMX configuration tooland not beeing able to use them together, to set up the hal...

Tobe by Senior III
  • 6582 Views
  • 8 replies
  • 0 kudos

FOC duration and Software error in MCSDK

Sir i am now working on STEVAL-SPIN3201 evaluation board having 6-step commutation method. I'm unable to rotate motor. I got errors like FOC duration and Software error. I also increased the execution rate one by one . still the motor is not rotating...

vishu by Associate II
  • 3251 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.