STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

How can I switch position mode to torque mode on SW?

Hi, I'm trying to use both position mode and torque mode.​I saw a comment saying when the position control is activated on a motor, the speed and torque control mode cannot be used.If so, can't it also be switched by turning the position control mode...

DWee.1 by Associate
  • 2696 Views
  • 3 replies
  • 1 kudos

JRE for MCSDK 5.4.8 MotorWorkbench?

I installed MCSDK 5.4.8 and CubeMX 5.2, which runs, so, if it uses Java, a suitable version must be installed.But when I try to Generate from a MotorWorkbench project, it gives me this error:Generation process failed. The embedded JRE was not found. ...

SKled.1 by Senior II
  • 1154 Views
  • 0 replies
  • 0 kudos

Resolved! Motor Pilot

I have an issue when using both PWMs generated by timers TIM2 and TIM3 to control two motors simultaneously. Specifically, when I call the function DC_MOTOR_Init(0), it activates PWM1, and when I call DC_MOTOR_Init(1), it activates PWM2. However, if ...

kkhli.1 by Associate III
  • 5309 Views
  • 4 replies
  • 2 kudos

Motor Profiler error

Hey,i have B-G431B-ESC1 board and Maxon motor. I can not profile this motor. I want to run my motor at 2000rpm max. Speed and 14V voltage source.The MC workbench is able to generate code. I am able to compile and program it using cube IDE.  i can con...

Jess32 by Associate II
  • 5312 Views
  • 4 replies
  • 1 kudos

STSPIN32F0B maximum electrical drive frequency?

What is the maximum electrical drive frequency that the ST provided firmware can achieve with the STSPIN32F0B IC?  And/or maximum RPM for a 5 pole pair motor?And the same question for the STPIN32G4....For a target frequency of about 1.5 kHz, what wou...

msch by Associate III
  • 4934 Views
  • 7 replies
  • 0 kudos

X-Cube MCSDK 6.2.0 and 6.2.1

Dear Sir/Madam ,I am currently using MCSDK 6.1.0 for generating BLDC motor control project for various type of BLDC motors in both FOC mode and HALL sensor mode operations.  Today I have tried to regenerate an existing BLDC motor control project  in ...

mkosu.2 by Associate
  • 1219 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.