STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Version Control & CI-CD with MC Workbench Project

Hi,I have done version control and CI-CD for large-scale C & C++ projects but I am not sure how to do this for the STM32-based tools and projects generated.For the Motor Control Firmware Development task I am currently assigned, I need to develop a s...

smaiti by Associate III
  • 1055 Views
  • 0 replies
  • 0 kudos

ACIM and NUCLEO-G431RB

Hello Everyone,  I'm trying to perform a command for ACIM, I created the code generated by MotorControl Workbench 6.2.1 without any problems and I'm using the NUCLEO-G431RB kit..I'm analyzing the PWM signals on the oscilloscope together with a filter...

Doubt.png
Gabe by Associate
  • 1312 Views
  • 0 replies
  • 0 kudos

B-G431-ESC hall voltage pin

Hi, I am using B-G431-ESC to control a brushless motor. Using Arduino and simpleFOC, I am able to control the motor in open loop setup. When tried using hall sensors pins, i see that there is no voltage on 5v pin on the esc board. The multimeter show...

STM.png STM2.png

Resolved! STM32 MC SDK

I have an application that requires 3 BLDC motors and I was wondering if I could use a single STM32 micro to run all three motors using the MC software library to interface to the hardware drivers of each motor.

digilog by Associate II
  • 1584 Views
  • 1 replies
  • 0 kudos

PI控制调参

MCSDK5.4.8版本 相最大电流270A,采样电阻0.0009欧,Lq 0.0991mH,Ld 0.04115mH,定子电阻0.01974毫欧,三电阻采样,相电流采样放大倍数3,电机相移角295度,PWM  16000Hz, 扭矩环调参后电机轴抱死,无法启动。

sunboy_351_0-1703141662729.png sunboy_351_1-1703141714429.png

RS-485 Half-Duplex bi-directional ADDC

I am trying to use RS-485 bidirectional half-duplex with automatic data direction control to communicate with an application generated with MC Workbench. The problem is, the response from the motor control application is too quick to respond before t...

JELLY.1 by Associate II
  • 1237 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.