STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

ST Evaluation Board EVSPIN32G4

Motor Control Workbench 6.2.1 I Have using the above version Pilot software. i am getting Speed feedback Err in BLDC Motor application. before i was try Hall Sensor Position Sequence value find and fill it . but i can't solve this fault.  any one sup...

Six step BLDC Control(X-NUCLEO-IHM11M1)

Hi,We have been using the X-NUCLEO-IHM11M1 driver to drive a BLDC motor. We were trying to read encoder values from the motor. The driver experienced short circuits on two occasions despite receiving sufficient voltage i.e. 3.5V to operate the BLDC m...

_Danny_ by Associate III
  • 717 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G4 BLDC HALL SENSOR

Hi,I am making a project using stm32cubeide for BLDC motor with Hall sensor.First project generated using timer2 made for Hall sensor reading with Combined Channel XOR ON / Hall Sensor Mode option, motor is working correctly, interrupting reading Hal...

kulfi27 by Associate II
  • 7245 Views
  • 4 replies
  • 1 kudos

STM32F411E-DISCO BLDC HALL SENSOR

Hello,With STM32F411E-DISCO, I am trying to obtain the RPM value by receiving data from the hall sensor of the BLDC motor. For this, I activated XOR On / HALL EFFECT Mode and connected the pins of the hall sensors to the relevant places.HAL_TIMEx_Hal...

sheqom by Associate III
  • 1349 Views
  • 0 replies
  • 0 kudos

Mini BLDC Torque Control

Hello. I am currently doing R&D work on controlling a 1 pole-pair, 12V BLDC motor. The controller I have chosen for my application is the B-G431-ESC1, and I am using Motor Control Workbench 6.2.1 to configure my controller. Currently, I am running in...

TS-LMG by Associate III
  • 5488 Views
  • 4 replies
  • 0 kudos

ODU Compressor Running Issues

Hi, I am using STEVAL-CTM010V1 to drive the compressor. I am using Workbench 5.4.7 for dual motor control. I am able to run the Drive2(Fan motor). when it is running, I am trying to run the compressor. Immediately, communication is getting disconnect...

VGani1_0-1701948738355.png
VGani.1 by Associate III
  • 3113 Views
  • 5 replies
  • 0 kudos

Can DC motor work more smoothly by timer dithering?

Hi guys,I am reading the timer dithering mode in the stm32 manual however I can't understand it very well.From my manual, the timer dither is for increasing the PWM resolution.According to my understanding, I can give the following example:Example: A...

Junde by Senior III
  • 1978 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.