STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! HSO Requirement

[VERSION]: MCSDK 6.2.0 [TOOL]: MC Workbench [DETAILS]: HiI want to prototype the HSO algorithm to compare the performance with the current Observer.From a webinar I have followed last month, the requirement were:- Analog inputs all 3 motors phase vol...

backb0ne by Associate II
  • 11153 Views
  • 6 replies
  • 2 kudos

PID Tuning - TORQUE CONTROL

Hi,In the document UM1052 page 37, it indicates that K_P/K_I = Ls/Rs for pole-zero cancellation in Figure 28. The question is whether this is the value to use for the ratio K_P/K_I , or should the motor control workbench be used to determine the valu...

jocelync by Associate II
  • 5105 Views
  • 6 replies
  • 0 kudos

MCSDK 6.2.0 is out!

Dear MCSDK users, MCSDK version 6.2 is now available: Download It here.Here are the main changes for this version:Hardware Compatibility : C0 Support for FOC 3-Shunt and 6 stepsH5 Support for FOC 3-Shunt and 1-ShuntAdd support of All MCUs part number...

Zied b. by ST Employee
  • 9426 Views
  • 8 replies
  • 2 kudos

IHM03 Gimbal Motor does not work with IHM08M1

Hi all,I have setup the demo project with the P-NUCLEO-IHM03 and I can start the motor using the Motor Pilot 6.2.1. So far so good. Since I want to use a stronger Motor eventually, I have bought the IHM-08 and want to use it with the Gimbal Motor as ...

MMenz.1 by Associate III
  • 3582 Views
  • 5 replies
  • 0 kudos

Resolved! MCSDK 6 STMCWB won't start

Hello.I'm trying to use MCSDK for EVLSPIN32G4-ACT demo board on Win7_x64 PC.After installing X-CUBE-MCSDK-FUL_6.2.1, MotorControl Workbench do not start at all.STMCWB.exe exits after splash screen without any notice,STMCWB_C.exe prints such error:......

Resolved! ST Evaluation Board EVSPIN32G4

Hi   i have recently purchased for ST Evaluation Board EVSPIN32G4   Supply voltage Nominal From 10 V to 75 VMaximum output current with heatsink (EVSPIN32G4) Peak 35 AContinuous(1)  20 Arms Maximum output current without heatsink (EVSPIN32G4NH) Peak ...

Resolved! MCSDK inverter

I'm using mcsdk and want to create an inverter file based on STM32G070CBTx, but when generating the project, it tells me that my selected hardware is not compatible with the algorithm

iskan by Associate III
  • 4004 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.