STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! STEVAL-ctm006V1 startup failure.

Hi,mcsdk: 6.2.1control board: nucleo-g474reBridge: XNUCLEO-IHM09M2Power Board: STEVAL-CTM009V1Motor: Motenergy ME1304 I prepared motor profile for ME1306 with help of EVSPIN32G4 and used in configuration,described above.But now I get Startup failure ...

tasifacij by Associate III
  • 4965 Views
  • 9 replies
  • 0 kudos

Resolved! Overcurrent protection hardware feature not showing

[VERSION]: 6.2.1[TOOL]: MC WB[DETAILS]:We are making a custom PCBA based on a STm32G474METx. Algorithm is FOC.I'm trying to activate Over current protection, but:My hwVariant is (parameters are not tuned/configured yet)"type": "SingleInput_RawCurrent...

LLang_0-1705396238928.png LLang_1-1705396572616.png
LLang by Associate
  • 2760 Views
  • 4 replies
  • 2 kudos

Space vector Modulation implementation

Hi GuysI have a question about space vector modulation implementation. I'm reading a code for ST MC workbench designed to run SVPWM. there is calculations for sector identification in space vector that I can't get it's idea completely. if someone ana...

photo9837570863.jpg photo9837570759.jpg

Resolved! Red flashing light when I connect my B-G431B-ESC1 board

Hi there, I recently purchased the B-G431B-ESC1 and when I connect it to my USB port, immediately a red flashing light appears. There are two other solid green lights. I am also not able to connect my ST-LINK to flash firmware, and this may be relate...

HudsonSam by Associate II
  • 11558 Views
  • 1 replies
  • 0 kudos

Resolved! How to change the PID Kp value

I am trying to tune a 28 pole 50V 20 Amp  motor 6 step  with hall sensors. Motor Pilot does not work for me. To get over this I am using STM32CubeMonitor to plot the speed response. I have also tried to change the values through Cube Monitor by writi...

Resolved! ZeST and HSO phase voltage filtering and ADC requirements?

I'm finalizing the design of a BLDC motor controller (up to 48V / 40A) and I'd like it to work well with HSO and (when available) ZeST.From other forum posts I've found the need for phase voltage measuring and to be able to capture these simultaneous...

StefanH by Associate III
  • 3222 Views
  • 3 replies
  • 1 kudos

STEVAL-PTOOL2V1 not work sample aplication

Hi please a can not build the sample application of STEVAL-PTOOL2V1.Have any newer version of application? I download this https://www.st.com/en/embedded-software/stsw-ptool2v1.html but not compile?what should I do ? I have to install something in cu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.