STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

motor open loop/closed loop control

hello everybody:    l'm currently debugging the FOC motor with MC Workbench.the development board model used is NUCLEO-G431RB and X-NUCLEO-IHM16M1.Now l have achieved closed-loop control of the motor through the encoder.Now l need to test the open-lo...

捕获.PNG 1.PNG
leo5 by Associate
  • 3696 Views
  • 2 replies
  • 0 kudos

Speed ramp with Potentiometer

"I'm trying to rotate the motor using potentiometer libraries. Do you think there are any other missing parts that I need to determine?" uint16_t potMeasArray[16]; potentiometerHandle.LPFilterBandwidthPOW2=4;potentiometerHandle.PotMeasArray=potMeasAr...

TKara.2 by Associate III
  • 2247 Views
  • 3 replies
  • 0 kudos

STSPIN BLDC motor control

I am looking for the development tool and software tools for this microcontroler. I found any tolls for the STM32 but not for the STSPIN.   Thanks for your comments.  

jopa by Associate
  • 1133 Views
  • 1 replies
  • 0 kudos

cubeMx with stspin32g4

i want to create a firmware for the stspin32g4 mcu but the cubeMx let me not select this mcu. in fact no spin mcu. i can not select a mcu with name spincubemx bug or st now not support the mcu with integrated drivers?

frankers by Associate II
  • 2934 Views
  • 3 replies
  • 0 kudos

MCSDK Encoder Alignment

Hi.I m new at ST MCSDK and i was reading some documents about mcsdk position control until waiting for my custom board arrive. I have few questions about encoder mounting and alignment operation.According to the documant AN5464; it seems that for fin...

qqwq.1 by Associate II
  • 1666 Views
  • 0 replies
  • 0 kudos

motor control workbench

In the latest version of the STM32 Motor Control Workbench (6.2.1), I am unable to select hall sensor-based speed control for my STM32 Nucleo F030R8 board with the IHM08M1 driver. Despite selecting hall sensor in the motor specifications, the option ...

#iR by Associate II
  • 1720 Views
  • 2 replies
  • 1 kudos

Resolved! 6-step speed fluctuation & current spikes

I am facing issues while running a BLDC motor using the 6-step algorithm on the STEVAL-SPIN3201 board. The only modification I have made is to the Hall effect sensor low-pass filter to address noisy input signals.I am encountering the following probl...

scope_47.png 1500rpm_no_load.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.