2024-02-19 9:17 AM
Hi there,
I recently purchased the B-G431B-ESC1 and when I connect it to my USB port, immediately a red flashing light appears. There are two other solid green lights.
I am also not able to connect my ST-LINK to flash firmware, and this may be related. But for that I am having issues installing the necessary drivers on my Windows10 laptop.
I have downloaded the relevant drivers and upon installation I am told that they were installed successfully, yet when I launch Device Manager I am not able to see them anywhere. Furthermore, when I try to launch the ST-link utility software I am told it is unable to launch because of some missing DLL files, namely mfc140.dll, VCRUNTIME140.dll, and MSVCP140.dll.
With a little online research on forums I see many suggesting I reinstall Visual C++ Redistributable. So I do that just (I remove what I had and installed Visual C++ Redistributable). But it did not help at all.
Any help to get me started with this board would be most appreciated. I have the issue with ST-link drivers which I am hoping would resolve the red flashing LED, but something tells me they may not be related.
Much appreciated.
Solved! Go to Solution.
2024-02-19 12:57 PM - edited 2024-02-19 12:58 PM
Problem resolved: Turned out to be incorrect cables. I was (unknowingly) using power-only USB cables (i.e. no data) and hence the blinking RED light.
2024-02-19 12:57 PM - edited 2024-02-19 12:58 PM
Problem resolved: Turned out to be incorrect cables. I was (unknowingly) using power-only USB cables (i.e. no data) and hence the blinking RED light.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.