STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! Rotor Position Measurement at Low Speeds

Hello,I am planning to use BLDC motors in a robotic manipulator where torque control of the motors will be established. Thus, FOC SDK of STMicroelectronics will be utilized. Since the manipulator will be a parallel one, none of the motors will need t...

Motor Profiler Error

Hi everyone. Following my Previous post, I have acquired a F446 Nucleo supporting 3shunt topology with the IHM17M1, such that I can perform motor profiling. However, I have run into an issue with the profiler getting stuck at 28%. Details are given b...

Motor Control SDK support H723ZG

Hello, We want to use the STMH723ZG with the Motor Control SDK. To do this I cannot find the .json file support for the board in the motor control workbench. Could I use another .json file from one of the fully-supported boards like the H745? Also, w...

hmantha by Associate
  • 322 Views
  • 1 replies
  • 0 kudos

STEVAL-CTM015V1 in sensorless mode

Hello, Is it possible to configure STEVAL-CTM015V1 to drive a 3-phase SRM (switched reluctance motor) in sensorless mode? The motor has no Hall sensors, and I cannot use the quadrature encoder signals because they are connected to a LabVIEW measureme...

bulcan10 by Associate
  • 497 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.