2026-02-18 2:50 AM
Hi,
Recently I have purchased ELSERVO1 board to drive BLDC Motors with 20A rated current. I dont have a ST Flasher, instead, I am using Nucleo g071rb board and removed the jumper pins in the board to flash the external ST controllers.
I have connected exact, pins in both the boards like, SWDIO, SWCLK, VDD and GND but, I am not able to flash the firmware saying ""Target no device found, Error in initializing ST-Link device" Reason: No device found on target"
What will be the issue in flashing the firmware?? I was able to flash to other boards.
I am suspecting that the ELSERVO1 board has dead..
please provide the solution.
2026-02-18 4:41 AM
The programmer software probably also expects you to connect NRST as well.
Regards
/Peter
2026-02-20 2:25 AM
I have tried connecting the NRST as well. The result remains same. What could be the problem. My development is stuck due to this...
2026-02-20 4:43 AM
Assuming you have connected every single wire, but you haven't mentioned where it gets its power supply from yet?
If it still doesn't work, have you tried programming another target using this ST-LINK/V2-1?
Regards
/Peter
2026-02-20 4:54 AM
Your assumption is right.. I have connected every single wire from Nucleo board STLink pins i.e VDD, SWDIO, SWCLK, NRST, GND pins to respective pins of ELSERVO1 board. ELSERVO1 Board has connected 24V DC supply and power LED is ON. Nucleo board is connected with USB cable.
Since I do not have a dedicated ST programmer, I am using this.. Which i have used to program our custom design ST board.
I hope, I have answered all your questions and doubts.
2026-02-20 5:35 AM
What programmer software did you try?
Was is set to Connect under Reset?
2026-02-23 8:59 PM
I am using STMCube IDE to program and flash the code. I think, I am not getting the solutions here properly. Could you please check the problem and provide the concrete solution.
2026-03-05 3:02 AM
My many questions may be frustrating, but you have provided too few details for concrete clues. It is still not clearly answered whether you were able to successfully program another target with the same ST-LINK on this NUCLEO-G071RB – because if CN4 is still plugged into the NUCLEO, the ST-LINK cannot program another target, as the STM32G071 of the NUCLEO is connected in parallel to the other target.
It would be best if you insert a photo of your setup using the camera button, showing the ST-LINK setting and the cable connection to the target.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.