STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Powerstep01 burned out

I am using Powerstep01 for stepmotor driving , comminucate with stm32H743 via SPI , and using x-cube-spn3's firmware for testing (IHM03A1_ExampleFor1Motor), but after initial function running , motor can not run. and after reset the power , powerstep...

powerstep_schematic.png
Ellison by Associate II
  • 472 Views
  • 6 replies
  • 0 kudos

Resolved! EVSPIN32G4: Current sense feedback resistor values

I all,I have a question regarding the EVSPIN32G4 board, specifically concerning the feedback resistors used in the current sensing network (default value: 11 kΩ).I am considering replacing them with 150 kΩ resistors. My main concern is whether this s...

JulesC by Associate III
  • 600 Views
  • 3 replies
  • 0 kudos

Resolved! source cord를 제공해 주실 수 있나요?

안녕하세요. 저는 개인 개발자 입니다. 이번에 steval ctm051 보드를 구입해서 srm 을 공부하려는 데 소스코드를 제공할 수 있다고 해서 어떻게하면 소스코드를 제공 받을 수 있는지 알려 주시면 감사하겠습니다. Please note that the forum is English-speaking, which is why I have machine-translated your question into English: Hello. I am a...

B-G431-ESC1 motor profiler connection

Hi, I'm trying to connect B-G431-ESC1 board, with no success. there is always : try to configure the boardI complile and flash a sample project successfully on the board. However still cannot connect motor profiler to make precision tuning of the mot...

Kamil1_0-1766945089159.png
Kamil1 by Associate III
  • 2609 Views
  • 29 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.