2024-12-21 10:53 AM
I can use a motor profiler with a custom board, but can I use a motor pilot with the same software? Is it possible to use a motor pilot with a custom board?
Solved! Go to Solution.
2025-01-06 12:52 AM
Hello TKara.2,
Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.
2025-01-06 12:52 AM
Hello TKara.2,
Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.
2025-01-06 6:40 PM
Thanks @Gael A
2025-02-20 2:34 AM - edited 2025-02-20 2:46 AM
Hi, I'm trying to do the same with a custom made board, i've selected the "motor Control option/tab" in the MC workbench, however when trying to builed the project in IDE i get the following error:
How can i resolve this issue?
I'm using the STM32G431RBT6
2026-03-08 1:39 AM
This is because not all the necessary paths to the libraries were automatically added. Check the include path in the project settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.