2025-08-11 7:45 AM
Hi all
static HAL_StatusTypeDef USB_CoreReset(USB_OTG_GlobalTypeDef *USBx)
{
__IO uint32_t count = 0U;
/* Wait for AHB master IDLE state. */
do
{
count++;
if (count > HAL_USB_TIMEOUT)
{
return HAL_TIMEOUT;
}
} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_AHBIDL) == 0U);
count = 10U;
/* few cycles before setting core reset */
while (count > 0U)
{
count--;
}
/* Core Soft Reset */
USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;
do
{
count++;
if (count > HAL_USB_TIMEOUT)
{
return HAL_TIMEOUT;
}
} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);
return HAL_OK;
}
at the USB_CoreReset function, my code keeps on getting stuck at the count++ and doesn't progress from there.
I have even included
RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // enable ULPI clock
before that function call but it does nothing.
My board is stm32u5g9.
Thank you and kind regards
Solved! Go to Solution.
2025-08-13 8:54 AM
The solution was
RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // OTG_HS PHY clock enable
RCC->APB3ENR |= RCC_APB3ENR_SYSCFGEN;
especially the last line of code
2025-08-13 8:54 AM
The solution was
RCC->AHB2ENR1 |= RCC_AHB2ENR1_OTGEN; // enable USB OTG HS clock
RCC->AHB2ENR1 |= RCC_AHB2ENR1_USBPHYCEN; // OTG_HS PHY clock enable
RCC->APB3ENR |= RCC_APB3ENR_SYSCFGEN;
especially the last line of code
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.