STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with memory sharing between cores

Hi Team, I'm new to STM32H7 controller. I've started exploring the shared memory in this dual core controller. I found a great one from MAJERLE. Thanks for that. I used the same concept and made a Flag to check for new data to read and write, it was ...

Resolved! USB CDC using USBX on F411

I am just a bit confused about how the CDC examples using USBX work. In the sample I've seen it seems that the code sets up some sort of UART to USB bridge. I think I don't need the UART and wanted to send and process data like the classic library us...

Use STM32H750 Internal Flash

I'm using STM32H750Is it possible to read and write like EEPROM in a specific part of the program (the last part of the internal flash area?)?I think it's impossible because there's only one sectorIf possible, I would appreciate it if you could give ...

SMj.1 by Associate II
  • 758 Views
  • 4 replies
  • 2 kudos

Resolved! USB CDC in STM32H563

tried to set up a USB device serial emulation (CDC) for STM32H563. Started a Free RTOS based project project in STM32CubeMX. But there I only can activate USB as "device_only in the "connectivity" segment but do not find any other USB related setting...

VKoen.1 by Associate II
  • 2602 Views
  • 4 replies
  • 0 kudos

STM32N6570-DK: LCD flickers when boot from flash

Hello,I have an application that shows image from camera from time to time on the screen. This app flashed at 0x7010'0000 and works well when I run FSBL in dev mode from debugger.But if I flash this FSBL at 0x7000'0000 and switch to flash boot app wo...

p5n by Associate II
  • 955 Views
  • 4 replies
  • 0 kudos

Resolved! X-CUBE-LED1642 download

The X-CUBE-LED1642 software seems to have gone missing. There are no links on the web page where you can download it.Should be here: https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32c...

qua by Senior
  • 559 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.