2025-09-17 12:59 PM
Hi,
I'm having a project that uses LTDC (565) UART4 (for printf debugging purposes) and ETH/LwIP.
The issue i'm having is an infinite loop in `LAN8742_Init` :
```
while(regvalue & LAN8742_BCR_SOFT_RESET)
```
always evalute to true and
```
if((pObj->IO.GetTick() - tickstart) <= LAN8742_SW_RESET_TO)
```
evalutes to true as well (tickstart is 0 and pObj->IO.GetTick() also returns 0).
STM32CubeMX warns me about possible conflicts with PIN - but I don't think LTDC and UART/ETH are using the same pins. Ater enabling ETH CubeMX warned about Clock but autoresolver fixed the issue.
2025-09-17 2:16 PM - edited 2025-09-17 2:25 PM
One of reasons can be failure of handshake with the PHY.
If you suspect conflict with other components, disable them and get the ETH working first.
> tickstart is 0 and pObj->IO.GetTick() also returns 0).
Maybe the PHY setup is broken too. Replace this to HAL_GetTick(). If HAL_GetTick keeps returning 0, the tick timer is broken. Too bad.
2025-10-24 12:15 AM
it looks like the ETH phy communication is failed, below is my ETH initial code on STM32H7S3:
const u8 ETH_HEADER_PACKET[] =
{
0x05, 0x04, 0x03, 0x02, 0x01, 0x00, // Destination Address, 6 bytes
// 0xFF, 0xFF, 0x00, 0x00, 0x00, 0x00, //
0x02, 0x00, 0x00, 0x00, 0x00, 0x00, // Source Address, 6 bytes, ETH_MAC_ADDR0~5
0x00, 0x04 // Length/type, 2 bytes
};
uint32_t idx, duplex, speed = 0;
ETH_MACConfigTypeDef MACConf;
ETH_MACFilterConfigTypeDef FilterConfig;
uint8_t macaddress[6]= {ETH_MAC_ADDR0, ETH_MAC_ADDR1, ETH_MAC_ADDR2, ETH_MAC_ADDR3, ETH_MAC_ADDR4, ETH_MAC_ADDR5};
EthHandle.Instance = ETH;
EthHandle.Init.MACAddr = macaddress;
EthHandle.Init.MediaInterface = HAL_ETH_RMII_MODE;
EthHandle.Init.RxDesc = DMARxDscrTab;
EthHandle.Init.TxDesc = DMATxDscrTab;
EthHandle.Init.RxBuffLen = ETH_RX_BUFFER_SIZE;
/* configure ethernet peripheral (GPIOs, clocks, MAC, DMA) */
HAL_ETH_Init(&EthHandle);
for(idx = 0; idx < ETH_RX_DESC_CNT; idx ++)
{
HAL_ETH_DescAssignMemory(&EthHandle, idx, Rx_Buff[idx], NULL);
}
memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD;
TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT;
/* Set PHY IO functions */
LAN8742_RegisterBusIO(&LAN8742, &LAN8742_IOCtx);
/* Initialize the LAN8742 ETH PHY */
if(LAN8742_Init(&LAN8742)!= LAN8742_STATUS_OK)
{
Error_Handler();
}
2025-10-24 3:57 PM
Well, then debug LAN8742_Init ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.