2017-09-18 12:27 AM
On the different STM32F4 Discovery boards with STM32F407 that we have here the serial number of the USB Virtual Port connection, as reported on the PC, is always 00000000001A.
Is this as it should be? Also, strange low number.
We also have another stm32f4 system with does have a 'real' serial number.
The actual question is how can I distinguish between usb connections when more systems are connected.
I need this to create a unique device name. This is in Linux, and udev rules are used to do this.
Normally I use the serial number for this, but what can I do now?
Thanks in advance,
Sietse
#stm32f4-usb-serial-number-virtual-com-portSolved! Go to Solution.
2017-09-18 1:46 PM
Hello!
Serial number of USB VCP is described as text inside usbd_desc.c file (or some other 'descriptor' file)
You can change this string to fit to your needs
Regards
vf
2017-09-18 1:46 PM
Hello!
Serial number of USB VCP is described as text inside usbd_desc.c file (or some other 'descriptor' file)
You can change this string to fit to your needs
Regards
vf
2017-09-19 12:41 AM
Thanks. I only looked in the Middleware directory for the string:(
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.