2017-09-21 6:18 AM
Unable to configure USB_DEVICE on STM32F070F6PX in STM32Cubemx.
STM32CubeMx version 4.22.1
Attempting to build a Virtual com.
Created cube project, configured USB port and Uart.
Added USB_DEVICE virtual com Middleware.
Basically everything you need to get a virtual com started.
Created and Iar EWARM project and compiled.
Looked at map file, project does not fit in ram memory.
Size of ram in map file is > 0x1800 the ram size of the part.
If I leave the middleware out it fits.
How would I use the USB as any of the device profiles without the middleware?
#unable-to-configure-usb_device-on-stm32f070f6px-in-cubeSolved! Go to Solution.
2017-09-21 4:32 PM
Hello!!
Goto usbd_cdc_if.c file and reduce the allocated ram size defined from following definitions
#define APP_RX_DATA_SIZE
#define APP_TX_DATA_SIZE
Regards
VF
2017-09-21 4:32 PM
Hello!!
Goto usbd_cdc_if.c file and reduce the allocated ram size defined from following definitions
#define APP_RX_DATA_SIZE
#define APP_TX_DATA_SIZE
Regards
VF
2017-09-22 7:24 AM
Thank you, that worked.
Looking closer, I was able to modify the APP_RX_DATA_SIZE and APP_TX_DATA_SIZE in the Cube configuration under Middleware.
I change it to 512 for both and it compile fine.
Probably a compliment to the ST developers, but I am so used to the basic configuration just compiling and working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.