2017-09-21 10:26 PM
Hi
All,
I have a problem after adding a new interface for stm32 USB-CDC. I receive wrong data after sending about 1250 bytes.
My code has:
a) Two interfaces generated from STM32 CubeMX:
. the first interface has one endpoint with address 0x82
. the second interface has two endpoints, bulk IN and bulk OUT, with addresses are 0x01 and 0x81
b) I add a new interface with two endpoints, bulk In and bulk OUT, with addresses are 0x03 and 0x83
This new interface runs well in sending some packages, and I receive correct data in about 1250 bytes. After that, I receive wrong data.
I run a simple experiment:
. sending a known eight bytes of a package in a loop in every 0.2 second. After 159 packages, I receive wrong packages. Each wrong package has twelve bytes ( I send only eight bytes!) and wrong data.
My code is generated from STM32 CubeMX version 4.22.0 USB, with freeRTOS, and using a development board, STM32 Nucleo-144 boards (NUCLEO-L496ZG).
Any idea or suggestion is very appreciated.
Jack
// ================= my code =========================================
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
// test
if (hUsbDeviceFS.dev_state != USBD_STATE_CONFIGURED)
return USBD_FAIL;
// end test
/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0){
return USBD_BUSY;
}
// test
for (int i = 0; i < Len; i++) {
UserTxBufferFS[i] = Buf[i];
}
// end test
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, UserTxBufferFS, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
/* USER CODE END 7 */
return result;
}
// =====================================================
void StartDefaultTask(void const * argument)
{
/* init code for USB_DEVICE */
osDelay(200);
MX_USB_DEVICE_Init();
osDelay(200);
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
// USB communication
if (hUsbDeviceFS.dev_state == USBD_STATE_CONFIGURED) {
if (recDataLength != 0) { // process a new request package
if ( (recData[1] == recData[2]) && (recData[1] == 99) ) {
isRequestSending = 1;
}
// finished processing one request package
recDataLength = 0;
}
}
if ( (hUsbDeviceFS.dev_state == USBD_STATE_CONFIGURED) && (isRequestSending == 1) ) {
uint8_t testBuf[8];
testBuf[0] = 8;
testBuf[1] = 3;
testBuf[2] = 0x0B;
testBuf[3] = TestCounter;
testBuf[4] = 4;
testBuf[5] = 0x08;
testBuf[6] = 1;
testBuf[7] = 0;
// send data
CDC_Transmit_FS(testBuf, 8);
//HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_7);
TestCounter++;
}
osDelay(200);
} // end for loop
/* USER CODE END 5 */
}
#usb #usb-new-interfaceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.