2025-06-18 5:32 AM
Hi STM32 community,
I have ordered those the Evalboards:
NUCLEO-G0B1RE
X-NUCLEO-SNK1M1 - USB Type-C Power Delivery Sink
2025-07-04 6:22 AM
2025-11-17 2:20 AM
Hi kuda1311
Thank you for sharing your .ioc and project.
On my end, using the same hardware as you (STM32G0B1RE and SNK1M1), regenerating a project from your .ioc, the application works as expected.
However, I reproduce your problem if I remove the JP4-RESET jumper from the SNK1M1 shied.
So, for use with STM32CubeMonitor-UCPD, the jumper configuration should be as follows:
- For the Nucleo power selection : Jumper JP2 on "STLink"
- For the SNK1M1 shield : Jumper JP4-RESET present and Jumper JP5-LDO_OUT present
-----------------------
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-04 4:39 AM
Hi, I a already Figured it out. But Thank you for the response. I have an other issue at the moment. I cant use the GPIOD, VSSI02 is on 3.3V. Im using stm32g0b1kb. It wont toggle it wont read, it does nothing. What am I missing.
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2025 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
void Check_VDDIO2_Status(void);
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
uint8_t rd10_switch_ready = 0;
volatile uint32_t current_time = 0;
volatile uint32_t previous_time = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
/* PWR-Clock sicherstellen (falls nicht schon in SystemClock_Config getan) */
__HAL_RCC_PWR_CLK_ENABLE();
/* VDDIO2 einmal definierte Reihenfolge: erst aus, dann an */
HAL_PWREx_DisableVddIO2();
HAL_Delay(10);
HAL_PWREx_EnableVddIO2(); // aktiviert die Domäne per Software
HAL_Delay(10); // etwas Wartezeit
Check_VDDIO2_Status(); // prüft das Status-Register
HAL_SYSCFG_StrobeDBattpinsConfig(SYSCFG_CFGR1_UCPD2_STROBE);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(iBIT1_GPIO_Port, iBIT1_Pin);
// GPIO_PinState p2 = HAL_GPIO_ReadPin(iBIT2_GPIO_Port, iBIT2_Pin);
// GPIO_PinState p3 = HAL_GPIO_ReadPin(iBIT3_GPIO_Port, iBIT3_Pin);
// GPIO_PinState p4 = HAL_GPIO_ReadPin(iBIT4_GPIO_Port, iBIT4_Pin);
/* Hier Breakpoint setzen und p1–p4 beobachten */
HAL_Delay(100);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* Ports aktivieren: hier minimal die Ports, auf denen deine iBIT-Pins liegen */
/* Wenn z.B. iBIT1 auf GPIOB, iBIT4 auf GPIOD liegt, musst du beide aktivieren. */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin : iBIT1_Pin */
GPIO_InitStruct.Pin = iBIT1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(iBIT1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : iBIT2_Pin iBIT3_Pin */
GPIO_InitStruct.Pin = iBIT2_Pin|iBIT3_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure GPIO pin : iBIT4_Pin */
GPIO_InitStruct.Pin = iBIT4_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(iBIT4_GPIO_Port, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI0_1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI0_1_IRQn);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* iBIT1: Interrupt-Eingang (Rising) */
GPIO_InitStruct.Pin = iBIT1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(iBIT1_GPIO_Port, &GPIO_InitStruct);
/* iBIT2: normaler digitaler Eingang */
GPIO_InitStruct.Pin = iBIT2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(iBIT2_GPIO_Port, &GPIO_InitStruct);
/* iBIT3: normaler digitaler Eingang (nicht analog, wenn du ihn lesen willst) */
GPIO_InitStruct.Pin = iBIT3_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(iBIT3_GPIO_Port, &GPIO_InitStruct);
/* iBIT4: normaler digitaler Eingang */
GPIO_InitStruct.Pin = iBIT4_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(iBIT4_GPIO_Port, &GPIO_InitStruct);
/* EXTI interrupt init – nur nötig, wenn iBIT1 auch wirklich an EXTI0_1 hängt */
HAL_NVIC_SetPriority(EXTI0_1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI0_1_IRQn);
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
void Check_VDDIO2_Status(void)
{
uint32_t sr2 = PWR->SR2;
/* Hier könntest du gezielt auf ein bestimmtes Bit prüfen, z.B.:
if (sr2 & PWR_SR2_PVMO2) { ... } */
if (sr2)
{
uint8_t a = 0;
(void)a;
}
else
{
uint8_t a = 1;
(void)a;
}
}
/**
* @brief EXTI line rising detection callback.
* @PAram GPIO_Pin: Specifies the pins connected EXTI line
* @retval None
*/
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
current_time = HAL_GetTick();
if ((GPIO_Pin == iBIT1_Pin) && ((current_time - previous_time) > 100))
{
rd10_switch_ready = 1;
previous_time = current_time;
}
else
{
rd10_switch_ready = 0;
}
}
/**
* @brief EXTI line falling detection callback.
* @PAram GPIO_Pin: Specifies the pins connected EXTI line
* @retval None
*/
void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
current_time = HAL_GetTick();
if ((GPIO_Pin == iBIT1_Pin) && ((current_time - previous_time) > 100))
{
rd10_switch_ready = 1;
previous_time = current_time;
}
else
{
rd10_switch_ready = 0;
}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.