2019-12-04 1:45 AM
Hello.
I cannot use Ethernet with my 2 weeks old NUCLEO-F767ZI (chip version Z).
Probably the LAN8742A does not work properly anymore.
After initilization I perform a check:
if (HAL_ETH_ReadPHYRegister(&heth, PHY_BSR, ®value)==HAL_OK) {
if (regvalue&0x04) {
// cable connected, but with this board never reached
...
}
}No LED of the connector is active.
The software works on other boards. (Latest FW, etc.)
Is there a chance to rescue the board?
Thank you Joerg
Solved! Go to Solution.
2019-12-14 8:57 AM
That is not a correct locally administered MAC address. As a minimum, the first byte must be 0x02. If that's the case, then the rest of the bits, except for multicast bit, can be whatever you want and the address is guaranteed to not interfere with universally administered addresses.
2019-12-14 9:10 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.