2026-02-19 7:47 AM
Oh boy, I'm frustrated...
Just when I thought I found the right MCU with the N6 (multi-channel audio over gigabit ethernet), I find in CubeMX and the datasheet that SAI2_SD_A and ETH1_CLK use the same pin. And I need both SAIs completely.
Very frustrating.
Using some I2S might be a solution, but these cannot be synced internally, aside from some other helpful features the SAIs have.
So, any other ideas, or will there be other packages where this pin-sharing problem might be solved?
Solved! Go to Solution.
2026-02-25 2:43 AM
Hi @LCE
Unfortunately, at this stage, there is no plan for additional STM32N6 package options to cover this case.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-20 2:13 AM
Hi @LCE
An internal ticket is submitted to dedicated team to check whether this is feasible. ( 227654)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-20 5:24 AM
Hi @LCE
After checking with our experts, an interesting audio solution is RTSP + PCM over ethernet : in VENC_RTSP_Server.
The application streams encoded H.264 video with optional audio.
To help you further, can you share more details about your multiple SAI usage?
Unfortunately, as you mentioned, SAI2_SD_A and ETH1_CLK I/O are sharing the same pin PF5 and cannot be used at the same time.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-20 5:37 AM
> VENC_RTSP_Server. I'll check that, thanks!
We need 2 SAIs and 2 blocks in each for 8 ADC channels.
Unfortunately, the ADCs we want to (/ must) use cannot work with TDM.
And using I2S... might be a PCB routing nightmare if done correctly considering EMI. (Apart from the fact that I had some problems on H7 using SAI and I2S in parallel and synced, some DMA issues I think)
2026-02-22 3:33 PM
The original title question - "N6: other packages in near future?" - I would be curious to know the answer to that question...
2026-02-22 10:46 PM
I agree, independent of my initial problem with the shared pin.
2026-02-25 2:43 AM
Hi @LCE
Unfortunately, at this stage, there is no plan for additional STM32N6 package options to cover this case.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.