2022-04-19 11:35 AM
Hi!
Problem:
I found a bug when I enabling the ETH perpherial in the STM32F407 processor. The error is a DMA bus error.
What's happening:
It occurs when the ethernet PHY recieve a message from my router.
How to produce the error:
I do the following steps to reproduce the error.
Then this call back function HAL_ETH_ErrorCallback(ETH_HandleTypeDef *heth); will be called.
The error code is a DMA error.
/** @defgroup ETH_Error_Code ETH Error Code
* @{
*/
#define HAL_ETH_ERROR_NONE ((uint32_t)0x00000000U) /*!< No error */
#define HAL_ETH_ERROR_PARAM ((uint32_t)0x00000001U) /*!< Busy error */
#define HAL_ETH_ERROR_BUSY ((uint32_t)0x00000002U) /*!< Parameter error */
#define HAL_ETH_ERROR_TIMEOUT ((uint32_t)0x00000004U) /*!< Timeout error */
#define HAL_ETH_ERROR_DMA ((uint32_t)0x00000008U) /*!< DMA transfer error */
#define HAL_ETH_ERROR_MAC ((uint32_t)0x00000010U) /*!< MAC transfer error */
#if (USE_HAL_ETH_REGISTER_CALLBACKS == 1)
#define HAL_ETH_ERROR_INVALID_CALLBACK ((uint32_t)0x00000020U) /*!< Invalid Callback error */
#endif /* USE_HAL_ETH_REGISTER_CALLBACKS */
/**
* @}
*/The DMA error is a DMA bus error.
This part of the code creates the DMA error code. See the arrow <---- HERE!
/* ETH DMA Error */
if (__HAL_ETH_DMA_GET_IT(heth, ETH_DMASR_AIS))
{
if (__HAL_ETH_DMA_GET_IT_SOURCE(heth, ETH_DMAIER_AISE))
{
heth->ErrorCode |= HAL_ETH_ERROR_DMA;
/* if fatal bus error occurred */
if (__HAL_ETH_DMA_GET_IT(heth, ETH_DMASR_FBES))
{
/* Get DMA error code */
heth->DMAErrorCode = READ_BIT(heth->Instance->DMASR, (ETH_DMASR_FBES | ETH_DMASR_TPS | ETH_DMASR_RPS)); <<--- HERE!
/* Disable all interrupts */
__HAL_ETH_DMA_DISABLE_IT(heth, ETH_DMAIER_NISE | ETH_DMAIER_AISE);
/* Set HAL state to ERROR */
heth->gState = HAL_ETH_STATE_ERROR;
}
else
{
/* Get DMA error status */
heth->DMAErrorCode = READ_BIT(heth->Instance->DMASR, (ETH_DMASR_ETS | ETH_DMASR_RWTS |
ETH_DMASR_RBUS | ETH_DMASR_AIS));
/* Clear the interrupt summary flag */
__HAL_ETH_DMA_CLEAR_IT(heth, (ETH_DMASR_ETS | ETH_DMASR_RWTS |
ETH_DMASR_RBUS | ETH_DMASR_AIS));
}My main function
/* Private variables ---------------------------------------------------------*/
ETH_TxPacketConfig TxConfig;
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */
void HAL_ETH_ErrorCallback(ETH_HandleTypeDef *heth){
uint32_t errorCode = heth->ErrorCode;
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_FSMC_Init();
MX_DCMI_Init();
MX_SPI2_Init();
MX_TIM1_Init();
MX_TIM3_Init();
MX_ADC1_Init();
MX_CAN1_Init();
MX_RTC_Init();
MX_TIM4_Init();
MX_UART5_Init();
MX_ETH_Init();
/* USER CODE BEGIN 2 */
/* Start up LCD */
HAL_GPIO_WritePin(LCD_RESET_GPIO_Port, LCD_RESET_Pin, GPIO_PIN_SET);
LCD_BL_ON();
lcdInit();
HAL_GPIO_WritePin(ETH_RESET_GPIO_Port, ETH_RESET_Pin, GPIO_PIN_RESET);
HAL_Delay(1);
HAL_GPIO_WritePin(ETH_RESET_GPIO_Port, ETH_RESET_Pin, GPIO_PIN_SET);
/* Enable interrupt */
HAL_ETH_Start_IT(&heth);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}Hardware settings
The hardware settings are for RMII for the Ethernet PHY DP83848 .
Yes! The LED D1 flashes when something happen at the network. The pin ACT_LED/COL should go low when something happens. The oscillator is at 50 MHz and very close to the DP83848 chip.
Software settings:
Download my project here:
STM32 project:
Schematic project (KiCAD):
Why I'm thinking this be a bug?
Because I have not configured ETH DMA and it give me a bug about that when my Ethernet PHY got a message and pass it over to the STM32 processor. I assume that STM32CubeIDE 1.9.0 have some issues then.
What am I 100% sure that I have been constructed the hardware correctly?
The Ethernet PHY address is 0x1 and I have been veryfied that this is correct address. The LED D1 is flashing when activity occurs at the network.
The callback function calls when the LED D1 flashes after initialization.
2022-04-30 10:41 AM
Internal ticket #126954. See in this thread.
This can take some time, let's wait until the holidays end. The last day of Ramadan is tomorrow.
2022-05-01 4:30 AM
Thank you for the information.
I will wait until a new update.
I write in this thread about the status.
2022-05-01 7:43 AM
> So there is a bug in STM32CubeIDE 1.9.0 for the F4 series about LwIP ... of the future fix?
Not a bug, but tenths of bugs, including a critical and non-trivial to fix ones. Not in a CubeIDE, but in a HAL drivers, CubeMX generated code and examples. And with a current attitude ST can fix those by the end of the century. But maybe I'm exaggerating and Pavel is more realistic - until we retire.
2022-05-01 7:49 AM
They fixed it in less than 24 hours. A mission impossible for ST!
2022-05-01 8:09 AM
I understand. Very bad for ST if their customers find out that there are bugs in their HAL-libraries. Very critical....
2022-05-01 3:23 PM
The bugs is fixed? I thought you said it would take a very long time?
2022-05-01 3:38 PM
Are you capable of reading what people write here and opening a link and reading the contents of that? Seems that no, because you didn't read the links I gave long ago also!
2022-05-01 3:41 PM
Sorry, I don't understand those links.
2022-05-01 7:20 PM
Maybe not critical at all. ST's product is chips, not the free software.
As far as they are confident that the hardware is solid (validated by internal tests, 3rd party proprietary software, partners) - no reason to worry,
2022-05-29 1:14 PM
@Pavel A. @Piranha
What's the status of ST's bug fix? Have you heard anything about this issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.