STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C read and write without stop condition

Using the HAL I2C library, is there any way to generate a continuous stream of scl and sda without a stop bit after the chip address acknowledge and data acknowledge. Otherwise I am planning to use a i2C bitbang library any recommendations? The targe...

0693W00000JP0LZQA1.png
VThan.2 by Associate III
  • 10253 Views
  • 15 replies
  • 0 kudos

How to enable serial-USB on B-L475E-IOT01A1 board?

I'm using the STM32 Io T discovery board (B-L475E-IOT01A1) to learn micro-ROS since this is a supported board with a demo use case.To flash the firmware on the board, the JP4 connector was set to 5V_ST_LINK pin and flashing was successful.The board a...

Ravi.N by Associate
  • 1038 Views
  • 1 replies
  • 0 kudos

Resolved! Where is BOOT_LOCK Option bit in 'G0x0?

All 'G0 except 'G06x/07x - i.e. including 'G0x0 - are in AN2606 described as Pattern 11; and Pattern 11 combinations involve BOOT_LOCK(bit).However, I see no BOOT_LOCK in the option bits in RM0454 rev.6.ST, please clarify.JW

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.